Downloads & Software-Updates


Category

Gira Expert

back

Order No. 0529 00, 2075 00

ZIP, 245.638 Kb

Version: 4.4.0

Date: 07.12.2015

Download

Expert Version 4.4.0

The Expert Software 4.4.0 is to be used in conjunction with the following end devices:

  • HomeServer 4
  • FacilityServer 4
  • HomeServer 3
  • FacilityServer 3
  • HomeServer 2
  • Iso for HS2.NET eliminated. This generation of devices cannot be supported any longer.

 

QuadClient / QuadConfig

Improvement

  • Extension of import function in QuadConfig
    Automated import of function templates, plugins and icons from the project backup when an existing project is used in a new version of the Expert Software or of QuadConfig.
  • Extension of function template Switching plus 1-101
    There is now the option to parameterise deviating texts when using the timer. Option: Deviating timer texts

 

Correction in QuadClient

  • Corrects an error, due to which the date display could not be correctly shown in French and Italian.
  • Corrects an error, due to which the "Lock" menu symbol stuck to the screen when scrolling.
  • Corrects an error, due to which the deactivation of timers via communication objects was incorrect in Polish.
  • Corrects an error, due to which the QuadClient reacted very slowly after it was not operated for a prolonged period.
  • Corrects an error in function template 1-122, due to which the slider was not operable at a step width between 0 and 1.
  • Corrects an error in the RSS feed reader plugin, due to which feeds without items generated an exception.
  • Corrects an error in the value display/weather station plugin, due to which offset tiles were displayed on positioning in first location in quadrants.

 

Corrections in QuadConfig

  • Corrects an error due to which the timer used was incorrectly assigned when importing function templates via the global library.
  • Corrects an error due to which the use of min. and max. boundary values in the communication object generated a warning.
  • Corrects an error in the function template "Switch plus 1-101", due to which an incorrect "Status on" symbol was used as default.
  • Corrects an error due to which the setting "Export to iPhone/iPad/Android" in the room was not correctly saved to the "Client_project.xml".
  • Corrects an error due to which the setting "Export to iPhone/iPad" in the room was not correctly saved to the "client_project.xml".
  • Corrects an error, due to which the configurations were not adopted after saving.
  • Corrects an error in the function template "Value input plus 1-125" due to which a min.-max. warning was generated, even though the boundaries were correct.
  • Corrects an error due to which the creation of a new project generated a fault message -> "No design was selected."
  • Corrects an error due to which the selection of step width "0" led to a fault message in the error log.
  • Corrects an error, due to which no data was saved, even though the order of subelements in a plugin had been changed.

 

Expert Software 4.4.0

  • Corrects an error, due to which no action was triggered, when an attempt was made to delete a used communication object via the delete button.
  • Corrects directories and version numbers of readme files.
  • Corrects an error due to which retentive data was lost as result of reprogramming.
  • Corrects a fault, due to which retentive data was not saved.
  • Corrects a fault in the translation of the English texts of the logic module "Heating – 9079" and "Cooling – 9087"