Downloads & Software-Updates


Category

Gira Project Assistant (GPA)

back

ZIP, 258.088 Kb

Version: 2.2

Date: 19.05.2017

Download

System requirements

Operating system: Windows 7, Windows 8, Windows 10
Free hard drive space: at least 16 GB
RAM: at least 4 GB


Supported devices

  • Gira X1 V1: Configuration/commissioning and maintenance functions
  • Gira Logic Module V1: Maintenance functions
  • Gira L1 V2: Configuration/commissioning and maintenance functions
  • Gira G1 V1: Maintenance functions
  • Gira KNX IP router V2: Firmware update
  • Gira KNX IP router V3: Maintenance functions

"Maintenance functions" refers to firmware updates, restarts and factory resets which are carried out through the Action Center (GPA menu -> Action Center).


Errors remedied in GPA v2.2

Logic is not executed

In some cases, logic may not have been executed. This error occurred if the device (Gira X1 or Gira L1) on which the logic was to be executed was deleted from the project and located again.

Error message "Project integration check failed"

Display of the error message "Project integration check failed" on start-up and on export of projects. This error message occurred in two situations and has been rectified in both cases:

  1. A function was named only with spaces.
  2. In the Gira X1 App v1.0 timers were created and deactivated. The runtime project was then downloaded from Gira X1 in the GPA and an attempt was made to start it up again.


Known errors in GPA V2.2

  • If the data type (KNX) in the group address table (not properties bar) is changed in the data point view and you then click directly on "Update", the setting is not adopted.
  • Please note that when entering the default value (data point view), the entered value is not checked. For a correct entry, please observe the example text and the tool tip. In addition, the entry is different to further entries, for example in the logic editor or timer editor. Please always comply with the format required by the editor.
  • Values that are written to a variable data point in simulation mode will not be passed on. This only applies to the simulation. The variable data points function as normal on the Gira L1.


Assistance

Gira X1/L1: Entry of device password

Before a device action is carried out, it is recommended that you unlock the device separately. This can be done in the "Building and devices" view (right-click on the device -> lock/unlock device).

Password for a Gira L1 after updating the firmware

When you have updated the firmware of a Gira L1 for which no password had been previously assigned or which has no device password sticker, the new password following a firmware update is "device".
Please change the device password during configuration.

Gira X1/L1: Device does not belong to the project

If a project is copied or read out of a device, or the project copy is loaded from the device, the physical device has to be connected to the device template again.
Click on the located device and then click on "Undo device assignment" in the properties bar. The device will be shown under "New devices found" again and can then be pulled back over to the device template.

OpenVPN and DHCP

The OpenVPN function in the Gira X1 only works in conjunction with DHCP. There must be a DHCP server in the network and the Gira X1 network must be initialised via DHCP and not by means of static IP configuration. This is necessary in order for the OpenVPN server to be able to assign an IP address to connecting clients. Should you wish to always use the Gira X1 with a fixed IP address, you can generally configure the DHCP server (usually part of the Internet router) in such a way that it always assigns the same IP address to the Gira X1.

Gira X1/L1: Saving retentive data

Retentive data is saved by the Gira L1 every 15 minutes. Data may be lost within this time period in the event of power failure.

Gira X1/L1: Provision of physical address requires application download

The Gira X1/L1 offers several physical addresses. When the physical address is programmed within the ETS, only the device address is adopted. The additional addresses are only adopted after downloading the application program.

Gira X1/L1: One-time delay for first event

After project download, the Gira X1/L1 responds to the first event with a delay of approx. 1 second.

GPA: Service "127.0.0.1" is not available“

A solution description is specified in the "Troubleshooting" directory. This is found in the installation directory of the Gira Project Assistant.
Example: "C:\Program Files (x86)\Gira\Gira Project Assistant\2.1\Troubleshooting"