Downloads & Software-Updates


Category

Gira Expert

Order No. 0529 00, 2075 00

ZIP, 255.714 Kb

Version: 4.5.0

Date: 10.11.2016

Download

Expert Software Version 4.5.0

The Expert Software 4.5.0 is to be used in conjunction with the following end devices:

  • HomeServer 4
  • FacilitiyServer 4
  • HomeServer 3
  • FacilityServer 3
  • HomeServer 2
  • Iso for HS2.NET eleminated. This generation of devices cannot be supported any longer.

 

QuadClient / QuadConfig

New features

  • Increased password security

 

Improvement


Basic setting of design selection
In the basic settings of QuadConfig the selection of active and inactive designs has been changed. From version 4.5.0:

  • Design 0 – active
  • Design 1 – inactive
  • Design 2 – active
  • Design 3 – inactive
  • Design 4 – active
  • Design 5 – active
  • Design 6 – active

 

Project check

  • Revised project check even when QuadConfig is running. Example: Changes to a communication object in Expert are directly adopted in QuadConfig without the need to restart the program.
  • Messages in the message window (error, warning, info) are reliable and synchronous, i.e. no display of ("wrong positive") error messages whose cause has already been "rectified".

 

Loading / saving projects

  • In rare cases it could occur that a project file was read incompletely – e.g. due to a defective function template having been loaded. Subsequent writing could then have led to data loss.
  • The read and write function for the project data was revised, the user will now be made aware of such errors. Written project data will only be adopted if successful.
  • In addition, log files can be opened from QuadConfig. In case of an error, these offer detailed information on the cause of the error.

 

Function template 1-107 – Shutters Awnings Roof window

  • Inverse motion direction for roof windows can now be selected as a response.

 

Function template 1-103 – Heating Plus (operationg mode switching)

  • "Presence button", "presence detector" selection options.
  • In the new "presence detector" mode, the buttons for operating mode switching are hidden.

 

Corrections

  • Fixed: Timer - Astro function - pop-up for offset setting Sunset does not open.
  • Fixed: Function template 1-108 -Sensor with limit: It was not possible to specify negative numbers as a limit.

 

Expert Software

New features

  • Increased password security

 

Corrections

  • Fixed: All EIB telegrams via EIBnet/IP coming from the HS have been marked as repetitions.

 

Gira verwendet Cookies für Websites in der Domain gira.de. Einige von ihnen sind essenziell, während andere uns helfen, diese Website und Ihre Erfahrung zu verbessern. Erfahren Sie mehr zu den von uns oder Dritten eingesetzten Cookies und Ihren Möglichkeiten diese auszustellen in unserer Datenschutzerklärung.

Wenn Sie Cookies zur statistischen Auswertung ablehnen, werden keine Tracking Cookies gesendet. Ihr Besuch auf dieser Website wird dann nicht erfasst.