Downloads & Software-Updates


Category

Gira Project Assistant (GPA)

ZIP, 409.208 Kb

Version: 3.0

Date: 01.10.2018

Download

System requirements

Operating system: Windows 7, Windows 8, Windows 10
Free hard drive space: at least 16 GB
RAM: at least 4 GB


Supported devices

  • Gira X1 V1: Configuration/commissioning and maintenance functions
  • Gira DCS IP data interface V1: Configuration/commissioning and maintenance functions
  • Gira Logic Module V1: Maintenance functions
  • Gira L1 V2: Configuration/commissioning and maintenance functions
  • Gira G1 V1: Maintenance functions
  • Gira KNX IP router V2: Firmware update
  • Gira KNX IP router V3: Maintenance functions
  • Gira S1: Maintenance functions

"Maintenance functions" refers to firmware updates, restarts and factory resets which are carried out through the Action Center (GPA menu -> Action Center).

What's new in GPA V3.0

  • Commissioning of the Gira door communication system via the Gira DCS IP data interface.
  • Readout of a Gira door communication system (existing system from 2016 or later) via the DCS IP data interface.
  • New instructions to make project start easier.
  • "New project" and "Maintenance and update" are opened with a single mouse click instead of a double click.
  • Gira X1 Scene set function: Assigning the scene set has been simplified.
  • Commissioning dialog has been revised.

Errors fixed in GPA V3.0

  • GPA crashed on closing when the PC was previously in sleep mode.
  • In some cases, the GPA crashed when setting up remote access via the Gira S1.
  • Translation errors rectified.

Assistance

OpenVPN and DHCP

The OpenVPN function in the Gira X1 only works in conjunction with DHCP. There must be a DHCP server in the network and the Gira X1 network must be initialised via DHCP and not by means of static IP configuration. This is necessary in order for the OpenVPN server to be able to assign an IP address to connecting clients. Should you wish to always use the Gira X1 with a fixed IP address, you can generally configure the DHCP server (usually part of the Internet router) in such a way that it always assigns the same IP address to the Gira X1.

Gira X1/L1: Saving retentive data

Retentive data is saved by the Gira L1 every 15 minutes. Data may be lost within this time period in the event of power failure.

Gira X1/L1: Provision of physical address requires application download

The Gira X1/L1 offers several physical addresses. When the physical address is programmed within the ETS, only the device address is adopted. The additional addresses are only adopted after downloading the application program.

Gira X1/L1: One-time delay for first event

After project download, the Gira X1/L1 responds to the first event with a delay of approx. 1 second.

GPA: Service "127.0.0.1" is not available“

A solution description is specified in the "Troubleshooting" directory. This is found in the installation directory of the Gira Project Assistant.
Example: "C:\Program Files (x86)\Gira\Gira Project Assistant\3.0\Troubleshooting"

Variable data points in the simulation

Values that are written to a variable data point in simulation mode will not be passed on. This only applies to the simulation. The variable data points function as normal on the Gira L1.

Firmware file cannot be added

If an error appears when adding a firmware file stating that the firmware file is not valid, there may be several causes for this, which are resolved as follows:

  • It is not an official firmware file or the file has not been downloaded correctly or fully. In this case, download the firmware file again from https://download.gira.de.
  • Not all the required Windows updates have been installed. In this case, install this update manually: https://www.microsoft.com/net/download/dotnet-framework-runtime/net462

Gira verwendet Cookies für Websites in der Domain gira.de. Einige von ihnen sind essenziell, während andere uns helfen, diese Website und Ihre Erfahrung zu verbessern. Erfahren Sie mehr zu den von uns oder Dritten eingesetzten Cookies und Ihren Möglichkeiten diese auszustellen in unserer Datenschutzerklärung.

Wenn Sie Cookies zur statistischen Auswertung ablehnen, werden keine Tracking Cookies gesendet. Ihr Besuch auf dieser Website wird dann nicht erfasst.