Downloads & Software-Updates


Category

Gira Expert

Order No. 0529 00, 2075 00

ZIP, 245.484 Kb

Version: 4.3.0

Date: 03.09.2015

Download

Expert Version 4.3.0

The Expert Software 4.3.0 must be used in conjunction with the following end devices:

  • HomeServer 4
  • FacilityServer 4
  • HomeServer 3
  • FacilityServer 3
  • HomeServer 2
  • Iso for HS2.NET eliminated. This generation of devices cannot be supported any longer.

 

Note

Update of firmware and QuadClient software required!

 

QuadClient/QuadConfig

Improvement

  • Revision of the conversion instructions for function template 5-20, Dimming without value display. Due to the conversion, the function template Dimming plus is now used for the function template 5-20.
  • Expansion of the function template 1-102, Dimming plus. The function of the function template 5-20, Dimming without value display, is now covered with the function template 1-102, Dimming plus.
    The function template 5-20 was moved into the area "Old (no use any more)".
  • Implementation of measures for securing the project data and avoiding data loss.

 

Corrections for function templates

  • Corrects an error, through which the plus and minus buttons are not shown in the HomeServer app for iPhone and iPad in the function template 5-20 "Dimming without value display".
  • Corrects an error, through which the saving of colours in the Colorpad of the colour control was no longer possible.
  • Corrects an error through which only values from 0-100 were transmitted in the colour control using the 3-byte object, instead of to KNX DPT 0-255.
  • Corrects an error through which the incorrect step size was carried out in the heating function template, 1-122 and 1-103, when the plus or minus button is pressed.
  • Corrects an error through which the combined white control was not possible in the colour control.
  • Corrects an error through which an inapplicable error message is shown in the value entry plus function template.
  • Corrects an error in the value entry plus function template. Due to deactivation of the "Permit value entry" option, no decimal places could be shown.

 

Corrections in plug-ins

  • Corrects an error through which the use of the camera plug-in was no longer possible in combination with a certain camera type.
  • Eliminates a problem through which no picture was shown in the camera plug-in.
  • Corrects an error through which it was not possible to show the hours display in the graph plug-in.
  • Corrects an error through which the DCS plug-in on Control 9 and Control 19 devices is shown in the middle following a door call.
  • Corrects an error through which the contents of the browser plug-in were only shown black when the plug-in was already opened and then were to be called again via a communication object.
  • Corrects an error through which the contents of the browser plug-in were only shown black. This took place as soon as the DCS plug-in was in quadrant and the browser plug- in was in another quadrant. Then an incoming door call was shown with the browser plug-in opened.
  • Corrects an error through which the DCS plug-in is not shown after the device has been restarted.
  • Corrects an error through which the axis marking in the graph plug-in was faulty.

 

Corrections in QuadConfig

  • Corrects an error through which an error message was triggered in the Expert software when a project without a QuadConfig configuration was to be transferred to the HS/FS.
  • Corrects an error through which changes to the communication object always affected the original and the duplicates after a function template had been duplicated on the "Visibility in room/function" slot.
  • Corrects an error through which changes to communication objects were not adopted in the QuadConfig when the QuadConfig was closed.
  • Corrects an error through which changes to the communication object by duplicated function templates were not adopted after the QuadConfig was closed once and opened again.
  • Corrects an error through which an error message was output after a project with QC visualisation was imported into the Expert software.
  • Corrects an error through which the building structure in the QuadClient was no longer shown when a project was imported and transferred to the HS/FS without changes in the QuadConfig.
  • Corrects an error through which the timer activated in the original was deactivated when duplicating function templates.

 

Expert software 4.3.0

Improvements

  • Adjustment of the behaviour with push notification activated without recipient groups. To transfer a project to the HS/FS with the push notification function activated, configured receiver groups are required to prevent unnecessary loading of the system.
  • Adding of a note information on the push notification function. This informs the user on the fact this it is necessary to activate the push notification function in the HomeServer portal.
  • Adjustment of the default error time for the push notification function. New default error times were specified to offer additional protection against loss of push messages. We recommend for existing projects that the error times used be checked and adjusted to the new error times from Version 4.3.0, if necessary.

 

Corrections

  • Corrects an error through which a scan error was shown on the debug page for all group addresses after scanning. This also occurred for the group addresses which had registered back correctly.
  • Corrects and error through which the incorrect texts in a popup of the graphic logic editor were shown in English.
  • Corrects an error through which the IP port configuration of cameras was impaired.
  • Correction of the documentation on the "Telegram delayer" logic node.
  • Corrects an error through which the Expert software froze after the serial project transfer.
  • Corrects an error through which the group address 0/0/0 was unintentionally transmitted on the bus.
  • Corrects an error through which the ISDN adapter no longer functioned and the HS/FS no longer sent calls.
  • Corrects an error through which several user settings were no longer available after deactivation of the "Call last settings" setting.

Gira verwendet Cookies für Websites in der Domain gira.de. Einige von ihnen sind essenziell, während andere uns helfen, diese Website und Ihre Erfahrung zu verbessern. Erfahren Sie mehr zu den von uns oder Dritten eingesetzten Cookies und Ihren Möglichkeiten diese auszustellen in unserer Datenschutzerklärung.

Wenn Sie Cookies zur statistischen Auswertung ablehnen, werden keine Tracking Cookies gesendet. Ihr Besuch auf dieser Website wird dann nicht erfasst.