Downloads & Software-Updates


Kategorie

Gira Expert

zurück

Order No. 0529 00, 2075 00

ZIP, 421.697 Kb

Version: 4.10.1

Date: 17.06.2020

Download

Archive

Language variants

Experte Version 4.10.1

System requirements

  • Operating system: Windows 7, Windows 8, Windows 10
  • Free hard drive space: at least 1 GB
  • RAM: at least 2 GB
  • Software platform: at least Microsoft .NET 4.5

Supported devices

The Expert Software 4.10.1 is to be used in conjunction with the following end devices:

  • Gira HomeServer 4
  • Gira FacilityServer 4

Update information

It is only possible to update to firmware version 4.10.1 from the following version:

  • 4.10.0.200117
  • 4.9.0.190612

Troubleshooting

Expert/firmware

  • Firmware versions 4.9.0 or 4.10.0 are required in order to update to version 4.10.1
    Gira HomeServers with index status <=I20 may no longer boot from a version earlier than 4.9.0.190612 after updating to firmware version 4.10.0.200117.
    Gira HomeServer can be made bootable again using a bootable USB stick containing version 4.8.0, 4.9.0 or 4.10.0. If at least firmware version 4.9.0.190612 is present, this step is no longer necessary.
  • The axis labels were not displaying correctly in diagrams in the user-defined visualisation (HS client, HTML visualisation or Ajax visualisation). This has been remedied with firmware version 4.10.1.200330.
  • The maximum size for camera images has been increased from 1 MB to 10 MB.

Note:
If you have already installed firmware version 4.10.0.200117 and do not make use of any user-defined visualisation including one or more diagrams with axis
labels, it is not necessary to carry out the firmware update. When uploading a project, no locking was incorporated.

QuadClient

  • When switching between different function views, parts of the most recently displayed view might also have been shown in the currently active view. This has been remedied with version 4.10.1.
  • Smaller values for switching times have been included for the dimmer function template in firmware version 4.10.0, as a result of which, switching times in existing projects have been offset. The 4.10.1 update corrects this offset, so that the set values will once again be transmitted.

Gira verwendet Cookies für Websites in der Domain gira.de. Einige von ihnen sind essenziell, während andere uns helfen, diese Website und Ihre Erfahrung zu verbessern. Erfahren Sie mehr zu den von uns oder Dritten eingesetzten Cookies und Ihren Möglichkeiten diese auszustellen in unserer Datenschutzerklärung.

Wenn Sie Cookies zur statistischen Auswertung ablehnen, werden keine Tracking Cookies gesendet. Ihr Besuch auf dieser Website wird dann nicht erfasst.